Hi,
I have made i.MX6D based design. Right now I am able to interface camera on MIPI CSI with 5MP OV5640. I would like to know what is the maximum camera resolution i.MX6D supports? And can I interface 10MP camera sensor with i.MX6D?
Thanks,
Mrudang
Hi Mrudang,
Please check previous thread about Mx6D and OV5640:
Question, i.MX6D/Q CSI input capability
Pixel resolution depen more on IPU, each IPU port can handle 150Mpixel/s, so 1920x720 pixel resolution at 60 fps ~ 83 pixel/s - it can be processed. I.MX6 has 2 IPU. IPU has 1 parallel and MIPI interfaces
Hope this helps
Hi,
Thanks for your reply.
I have gone through what you have shared me about CSI and IPU and still working on it.
Can you please let me know whether iMX6D/Q supports 10MP image sensor for capturing an image and video recording?
If yes, then which are camera image sensor are most suitable for iMX6D/Q. Please provide no#.
Thanks,
Mrudang