AnsweredAssumed Answered

Power tree issue

Question asked by wenming Feng on May 1, 2017
Latest reply on May 2, 2017 by wenming Feng

When the customer board boot into kernel.

The power supply is not what we expected.

how about the PMIC registers need to configure in DTS.

when I connect the mipi camera with imx6DL customer board. after booting into kernel.

ov564x_mipi: ov564x_mipi@3c { /* i2c1 driver */
compatible = "ovti,ov564x_mipi";
reg = <0x3c>;
clocks = <&clks 201>;
clock-names = "csi_mclk";
DOVDD-supply = <&vgen4_reg>; /* 1.8v */
AVDD-supply = <&vgen6_reg>; /* 2.8v, rev C board is VGEN3
rev B board is VGEN5 */
DVDD-supply = <&vgen2_reg>; /* 1.5v*/
pwn-gpios = <&gpio6 0 1>; /* active low: SD1_CLK */
rst-gpios = <&gpio6 1 0>; /* active high: SD1_DAT2 */
csi_id = <1>;
mclk = <24000000>;
mclk_source = <0>;
};

The AVDD is supposed to be 2.8V but I got 3.8V whether I change the reference to vgen6_reg or vgen3_reg in DT bold text above showing what I used.

PMIC settings is showing below. Shall I change the min=max=dedicated one, what I needed, eg 2800000?

Anybody else encounter this issue or what I missed for the pmic setting in DT?

 

pmic: pfuze100@08 {
compatible = "fsl,pfuze100";
reg = <0x08>;

regulators {
sw1a_reg: sw1ab {
regulator-min-microvolt = <300000>;
regulator-max-microvolt = <1875000>;
regulator-boot-on;
regulator-always-on;
regulator-ramp-delay = <6250>;
};

sw1c_reg: sw1c {
regulator-min-microvolt = <300000>;
regulator-max-microvolt = <1875000>;
regulator-boot-on;
regulator-always-on;
regulator-ramp-delay = <6250>;
};

sw2_reg: sw2 {
regulator-min-microvolt = <800000>;
regulator-max-microvolt = <3300000>;
regulator-boot-on;
regulator-always-on;
regulator-ramp-delay = <6250>;
};

sw3a_reg: sw3a {
regulator-min-microvolt = <400000>;
regulator-max-microvolt = <1975000>;
regulator-boot-on;
regulator-always-on;
};

sw3b_reg: sw3b {
regulator-min-microvolt = <400000>;
regulator-max-microvolt = <1975000>;
regulator-boot-on;
regulator-always-on;
};

sw4_reg: sw4 {
regulator-min-microvolt = <800000>;
regulator-max-microvolt = <3300000>;
};

swbst_reg: swbst {
regulator-min-microvolt = <5000000>;
regulator-max-microvolt = <5150000>;
};

snvs_reg: vsnvs {
regulator-min-microvolt = <1000000>;
regulator-max-microvolt = <3000000>;
regulator-boot-on;
regulator-always-on;
};

vref_reg: vrefddr {
regulator-boot-on;
regulator-always-on;
};

vgen1_reg: vgen1 {
regulator-min-microvolt = <800000>;
regulator-max-microvolt = <1550000>;
};

vgen2_reg: vgen2 {
regulator-min-microvolt = <800000>;
regulator-max-microvolt = <1550000>;
};

vgen3_reg: vgen3 {
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <3300000>;
};

vgen4_reg: vgen4 {
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
};

vgen5_reg: vgen5 {
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
};

vgen6_reg: vgen6 {
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
};
};

 

Thanks!

 

Wenming

Outcomes