Hi,
We have a requirement to connect a 32 bit data bus supported device on T1022 local bus. Since the Processor (T1022) supports 16 bit data bus , can we connect this device (32bit data bus) on Processor eLBC. If yes, what changes need to be incorporated to make it work.
Regards
Ram
> can we connect this device (32bit data bus) on Processor eLBC.
Sorry, which "Processor eLBC" is in question?
T1022 has only IFC controller supporting 16-bit data bus.
Yes, it is IFC controller. Apologies for the inconvenience.
Can it be used to connect 32 bit data bus supported device ?
Regards
Ram
> Can it be used to connect 32 bit data bus supported device?
There is no direct way to connect 32-bit-wide device to the IFC.
I assume that it is possible to use a CPLD/FPGA, so IFC in GASIC mode will be able to communicate with the 32-bt-wide device.
Hi,
Thanks for the update.
Do we need to incorporate any changes in software/BSP to support the 32-bit wide device ?
Will there be any performance degradation for the 32-bit wide device ?