Hello,
I am having problems with interrupts for the 1588 timer. Even with EIR[TS_TIMER] asserted and EIMR[TS_TIMER] unmasked, my interrupt handler is not called. I have performed and verified the following steps:
I am also fairly certain that my interrupt handler is configured correctly since I can use PSR214[SWTN] to trigger the handler manually.
Is there any additional operations that needs to be performed for the TS_TIMER interrupt to trigger the interrupt vector? I am testing on ENET0 and the system is using eCos as OS if that makes any difference.
Best regards,
Johannes
Solved! Go to Solution.
Hi Johannes,
it looks similar as this one...https://community.nxp.com/thread/438400
Try to use vector #210 (ENET group 0)
BR, Petr
Hi Johannes,
it looks similar as this one...https://community.nxp.com/thread/438400
Try to use vector #210 (ENET group 0)
BR, Petr
Thank you Petr, I had missed that #210 was timer-related and assumed #214 was the one I needed.
BR, Johannes