AnsweredAssumed Answered

Disabling the functions to carry out the initialization of RW and BSS data sections

Question asked by Pablo Igor Vicente on Apr 27, 2017
Latest reply on May 15, 2017 by Pablo Igor Vicente

Hi,

 

Working with 8-bit microcontrollers and CodeWarrior the define __ONLY_INIT_SP is used to enable or disable the execution of Init() function in the startup routine; in order to enable or disable the initialization of zero out RAM areas and copy initialization data from ROM to RAM.

 

My question is:

Working with kinetis and MCUXpresso, how can I disable the execution of the functions to carry out the initialization of RW and BSS data sections?

 

Thanks in advance

Outcomes