LS1021 QUICC Engine Microcode Usage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1021 QUICC Engine Microcode Usage

Jump to solution
1,446 Views
pratapgaikwad
Contributor I

Hello,

I downloaded QE microcode for LS1021 from NXP git repository. But I do not know how to use it.
http://git.freescale.com/git/cgit.cgi/ppc/sdk/qe-ucode.git/log/?h=sdk-v2.0.x

Can anybody please let me know :

1. how and where to upload the microcode ?

2. Initialization steps for QE on LS1021?

3. Is there any application note ? I am planning to use QUICC Engine UART interface.

Labels (1)
0 Kudos
1 Solution
1,160 Views
Pavel
NXP Employee
NXP Employee

Use NXP SDK Linux for LS1021a:

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/qoriq-layerscape-arm-proc...

 

This SDK supports UCC UART for LS1021a boards.

See attached .dts file.


Have a great day,
Pavel Chubakov
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
1,161 Views
Pavel
NXP Employee
NXP Employee

Use NXP SDK Linux for LS1021a:

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/qoriq-layerscape-arm-proc...

 

This SDK supports UCC UART for LS1021a boards.

See attached .dts file.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos