I'm working on i.MX6 board. I need to configure SPI for ATMEL mXT1664S-AT touch controller. Please suggest me how to configure. Also, please verify the following entry in the device tree. FYI, kernel version 4.1.15-2.0.0.
touch: mXT1664S-AT@0 {
compatible = "atmel,maxtouch";
reg = <0>;
spi-max-frequency = <8000000>;
};
Are these properties enough to configure or do I need to add any other property?
Here I attached an introduction to device tree.
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------