Help Bringing I.MX6UL Board To Life

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help Bringing I.MX6UL Board To Life

745 Views
nachodiz
Contributor III

Dear all, we´re trying to bring out board to life (for an important Automotive Customer)

MOV_0775.mp4 - Google Drive 

I´tried to connect through serial downloader (USB) and it hangs when Loading Uboot

We also have UART pads Just in case for debug

My intention it´s to copy the i.MX6UL-EVK Fuses but changuing the SD2 boot device  from SD1 (we have the sd on the SD1 bus)

Who can help us with this process, STEPS....
I want to perform a DDR Test

King Regards

Labels (1)
0 Kudos
3 Replies

535 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

   Looks like the MFG system (U-boot, kernel, ramfs) can be loaded (maybe successfully ),

but cannot  start, since reset takes place. This  may be memory bug. Please try the DDR stress test.

https://community.nxp.com/docs/DOC-105652 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos

535 Views
zzx
Contributor I

Hello,

      My  i.MX6UL-EVK board has meet the same problem like the video ,  and I try the DDR stress test but failed.

      The board is working correctly before , but yesterday it suddenly unable to work.

 

      pastedImage_3.png

      How can I solve the problem or How can I test the board to determine that whether the board is dead?

      Thanks a lot for your help.

0 Kudos

535 Views
nachodiz
Contributor III

The board works ok it pass calibration, ddr stress and now while running mfgtool through SERIAL DOWNLOADER USB, the uart outputs the boot sequence

here calibration results:
RES.zip - Google Drive 
Here the uart output:

aaa.png


This data does not correspond with my board (i have 512mb ddr3) and 528 Mhz

0 Kudos