Hi All,
This is hmyang.
I have a problem about android_M6.0.1_2.1.0 when the device is started as like title.
HW Information : iMX6DL SABRE AUTO PDK Board
SW platform : android_M6.0.1_2.1.0, SW is stored in HC-SD Card
When this log , "binder: 176:176 transaction failed 29189, size 0-0 ", is always happened, PDK Board is stopped.
I will attach the full log file.
Please help to resolve this issue.
Regards
HM
Original Attachment has been moved to: log-binder-176-176-transaction-failed-29189-size-0-0.txt.zip
Solved! Go to Solution.
Hi Yang,
Please check following block with a possible post solution for android binder issues:
Avoiding binder issue on android pre-built image - i.MXDev Blog
Hope this helps
Hi Yang,
Please check following block with a possible post solution for android binder issues:
Avoiding binder issue on android pre-built image - i.MXDev Blog
Hope this helps
Hi All,
Boot print command is as below :
================================
U-Boot 2015.04 (Apr 26 2017 - 13:48:19)
CPU: Freescale i.MX6DL rev1.1 at 792 MHz
CPU: Temperature 42 C
Reset cause: POR
Board: MX6Q-Sabreauto revA
I2C: ready
DRAM: 2 GiB
PMIC: PFUZE100 ID=0x10
NAND: 0 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
flash target is MMC:1
Fastboot: Normal
Net: FEC [PRIME]
Hit any key to stop autoboot: 0
=> print
baudrate=115200
bootargs=console=ttymxc3,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off vmalloc=320M androidboot.console=ttymxc3 consoleblank=0 androidboot.hardware=freescale cma=384M androidboot.selinux=disabled androidboot.dm_verity=disabled
bootcmd=boota mmc1
bootdelay=1
ethact=FEC
ethaddr=00:04:9f:03:51:32
ethprime=FEC
fastboot_dev=mmc1
fdt_high=0xffffffff
initrd_high=0xffffffff
loadaddr=0x12000000
splashpos=m,m
Environment size: 495/8188 bytes
=>
======================================
I already setup androidboot.dm_verify to disabled
Is there any issue in my boot print command?
Please help to resolve this issue.
Regards
HM