AnsweredAssumed Answered

PF0100 Default configuration

Question asked by Abhijit Mote on Apr 26, 2017
Latest reply on Apr 30, 2017 by Artur Petukhov

1. In default mode of PF0100 there is no mention about the following supplies:

SWBST_VOLT, VGEN1_VOLT and VGEN3_VOLT. Does it mean that these supplies are not enabled?

2. Default configuration of register SWBSTCTL as per data sheet says the SWBST_VOLT is configured as 'ON' and configured for 5.0V.

3. For LDO's there are 4 bits (3:0) for output setting marked as VGENx (Register VGENxCTL) and its default value is mentioned as 0x80. The maximum value 4 bits can achieve is 0x0F. Is this a typing mistake? 

 

Refer the attachment below for more details.

Attachments

Outcomes