PCIe to Nexus adapter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCIe to Nexus adapter

846 Views
miguelgarciacle
Contributor I

Are there any PCIe to Nexus connector adapters?

For advanced debugging, a Nexus / Aurora high speed debugging interface is needed. For this, some of the SerDes lanes are taken to the dedicated 70-pin connector. This is done in some boards, such as the T2080QDS-PA board.

However, many reference design boards take the corresponding SerDes lanes to a PCIe connector. That is the case for the T2080RDB or the T1040RDB boards.

Looking at the schematics of the T1040RDB PCIe port and at the standard pinout of the Nexus interface, I see that almost all if not all the Nexus signals are available at the PCI-Express connector.

Is there an adapter from the PCIe connector to the 70-pin Nexus / Aurora connector?

Labels (2)
0 Kudos
2 Replies

570 Views
MatthiasB
Contributor II

I found this question by accident and it's maybe too late for Miguel Garcia Clemente,

but Lauterbach provides a solution to trace over PCIe using an adapter card.

Regards,

Matthias

0 Kudos

570 Views
ufedor
NXP Employee
NXP Employee

There is no such adapter.

0 Kudos