Hello,
I've installed and activated lpcexpresso 8.2.2 in my macbook. Then, trying to flush blink example, I've got an error.
This error has appeared as well when I tried to boot manually:
bash-3.2$ ./dfu-util -d 0x471:0xdf55 -c 0 -t 2048 -R -D LPCXpressoWIN.enc
dfu-util 0.9
Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.
Copyright 2010-2016 Tormod Volden and Stefan Schmidt
This program is Free Software and has ABSOLUTELY NO WARRANTY
Please report bugs to http://sourceforge.net/p/dfu-util/tickets/
dfu-util: Invalid DFU suffix signature
dfu-util: A valid DFU suffix will be required in a future dfu-util release!!!
dyld: lazy symbol binding failed: Symbol not found: _OSAtomicIncrement32Barrier
Referenced from: /Applications/lpcxpresso_8.2.2_650/lpcxpresso/bin/./libusb-1.0.0.dylib
Expected in: /usr/lib/libSystem.B.dylib
dyld: Symbol not found: _OSAtomicIncrement32Barrier
Referenced from: /Applications/lpcxpresso_8.2.2_650/lpcxpresso/bin/./libusb-1.0.0.dylib
Expected in: /usr/lib/libSystem.B.dylib
Trace/BPT trap: 5
bash-3.2$
Is it possible to continue working with LPCExpresso board in my environment?
Stan
On further investigation we can see that you have identified a compatibility issue between LPCXpresso IDE 8.2.2 and Mac OSX 10.9.5.
Unfortunately the options available are to downgrade your version of LPCXpresso IDE to version 7.9, or to upgrade the version of OSX running on your Mac.
Yours,
LPCXpresso Support
Initially I suggest you take a look at the following FAQ https://community.nxp.com/message/630541 this provides some background and a trouble shooting section.
Yours
LPCXpresso Support