Does i.MX287 supports PWM inputs?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does i.MX287 supports PWM inputs?

458 Views
sourabhzunke090
Contributor I

How do we read digital pulses from encoders which can have a frequency range 1Hz to 15KHz on i.mx287. The reference manual for i.mx287 has information about the PWM output pins and doesn't mentions anything about reading PWM inputs. Does i.mx287 cannot read PWM inputs.

What is the possible solution to read PWM inputs if i.mx287 doesn't supports it?

Can it be done using HSADC?

Does other SoM in i.MX series support PWM inputs? 

Can I read PWM inputs of the specified range using external peripherals which gives output understandable to i.MX287?

Labels (4)
Tags (2)
0 Kudos
1 Reply

333 Views
igorpadykov
NXP Employee
NXP Employee

Hi sourabh

please check Chapter 23 Timers and Rotary Decoder (TIMROT)

i.MX28 Reference Manual

http://cache.freescale.com/files/dsp/doc/ref_manual/MCIMX28RM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------