USB OTG connection diagram

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB OTG connection diagram

Jump to solution
687 Views
javierhernande1
Contributor IV

Hello,

Is there an example of how to connect K2x MCU family to USB Type-C connector with OTG support? I have not found anything.

Best regards

usb.png

Labels (2)
1 Solution
426 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Javier,

If you need full USB type C function support, you have use some chip like CC logic for USB Type-C applications|NXP besides Kinetis K2x, but if you just need a USB type C connection, you may connect the signals that K2x USB FS OTG has and leave other unused signals unconnected.

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
427 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Javier,

If you need full USB type C function support, you have use some chip like CC logic for USB Type-C applications|NXP besides Kinetis K2x, but if you just need a USB type C connection, you may connect the signals that K2x USB FS OTG has and leave other unused signals unconnected.

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

426 Views
javierhernande1
Contributor IV

just at a USB type C connection.

Thanks very much.

0 Kudos