i.MX 6SoloX SABRESDB Dev Board Boot from NFS and TFTP boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 6SoloX SABRESDB Dev Board Boot from NFS and TFTP boot

700 Views
anilchowdary
Contributor II

Hi,

 I have problem with booting from TFTP and NFS instated of SD-card  and I had followed Yocto NFS & TFTP boot  link but struck and continuously monitoring eth0 and eth1 connection.

Error:

input: gpio-keys as /devices/soc0/gpio-keys/input/input7
snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:01 UTC (1)
fec 2188000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=2188000.ethernet:01, irq=-1)
IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
fec 21b4000.ethernet eth1: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=2188000.ethernet:02, irq=-1)
IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
fec 2188000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
Sending DHCP requests ......
random: nonblocking pool is initialized
timed out!

Please help on this, if you have proper boot arguments, please share with us.

waiting for your valuable support.

Thanks & Regards

-Anil

Labels (1)
0 Kudos
1 Reply

555 Views
igorpadykov
NXP Employee
NXP Employee

Hi Anil

please refer to sect.4.7.5 Running the Linux image from NFS

attached Linux Guide and use i.MX6SX SabreSD Demo Image

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0_iMX6SX&appType=license&location=null&Parent... 

BSP:

http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/?id=rel_imx_4.1.15_2.0.0_ga&h=imx_4.1.1...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos