Board not booting after closed even with HAB events

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Board not booting after closed even with HAB events

1,192 Views
jaganteki
Contributor I

I was able to succeeded with signed boot on u-boot with u-boot.imx.

=> hab_status
Secure boot disabled
HAB Configuration: 0xf0, HAB State: 0x66

<< series of HAB events >>

After that I close the device
=> fuse prog 0 6 0x2

But board is not able to boot with signed image or normal image, any help?

Labels (1)
0 Kudos
6 Replies

909 Views
jaganteki
Contributor I

Hi,

Issue is that, somehow I lost the CST key so I'm unable to make proper signed image. Is there any possibility to boot the board like with JTAG or any other way.

And also once the device is closed (secure), we can't revert to un-secure is it?

thanks!

Jagan.

0 Kudos

909 Views
gary_bisson
Senior Contributor III

Hi,

Yes if you haven't burned any other fuse you should be able to use the JTAG just fine.

And no, of course, you can't revert a close device otherwise it wouldn't be secure.

Regards,

Gary

0 Kudos

909 Views
jaganteki
Contributor I

Hi,

This is the full hab_status

=> hab_status

Secure boot disabled

HAB Configuration: 0xf0, HAB State: 0x66

--------- HAB Event 1 -----------------
event data:
        0xdb 0x00 0x08 0x41 0x33 0x11 0xcf 0x00

STS = HAB_FAILURE (0x33)
RSN = HAB_INV_CSF (0x11)
CTX = HAB_CTX_CSF (0xCF)
ENG = HAB_ENG_ANY (0x00)


--------- HAB Event 2 -----------------
event data:
        0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00
        0x00 0x00 0x00 0x00 0x00 0x90 0x74 0x00
        0x00 0x00 0x00 0x20

STS = HAB_FAILURE (0x33)
RSN = HAB_INV_ASSERTION (0x0C)
CTX = HAB_CTX_ASSERT (0xA0)
ENG = HAB_ENG_ANY (0x00)


--------- HAB Event 3 -----------------
event data:
        0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00
        0x00 0x00 0x00 0x00 0x00 0x90 0x74 0x20
        0x00 0x00 0x00 0x01

STS = HAB_FAILURE (0x33)
RSN = HAB_INV_ASSERTION (0x0C)
CTX = HAB_CTX_ASSERT (0xA0)
ENG = HAB_ENG_ANY (0x00)


--------- HAB Event 4 -----------------
event data:
        0xdb 0x00 0x14 0x41 0x33 0x0c 0xa0 0x00
        0x00 0x00 0x00 0x00 0x00 0x90 0x80 0x00
        0x00 0x00 0x00 0x04

STS = HAB_FAILURE (0x33)
RSN = HAB_INV_ASSERTION (0x0C)
CTX = HAB_CTX_ASSERT (0xA0)
ENG = HAB_ENG_ANY (0x00)

0 Kudos

909 Views
Yuri
NXP Employee
NXP Employee

Hello.

  below is similar issue :

https://community.nxp.com/message/486597?commentID=486597#comment-486597 

Hope it helps.

Regards,

Yuri.

0 Kudos

909 Views
Yuri
NXP Employee
NXP Employee

Hello,

  What are the mentioned "<< series of HAB events >>" ?

Regards,

Yuri.

0 Kudos

909 Views
gary_bisson
Senior Contributor III

Hi Jagan,

I think you didn't understand the HAB Events, you can think of the events as ERRORS.

So having HAB events, you shouldn't have closed the device.

Now the only option is to properly sign a binary to load using the serial download protocol (imx_usb_loader) or to use a JTAG.

Regards,

Gary

0 Kudos