i.MX6 PCIe use iATU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 PCIe use iATU

1,081 Views
tomohisa_sakamo
Senior Contributor II

Dear Support-team,

We would like to extend PCIe connection using i.MX 6 iATU.
We want to program by referring to technical documents such as specifications of iATU.
We are already referred I.MX 6 RM, patch etc to in the community.

1)Can you disclose detailed information on i.MX 6's iATU?

2)Or we could refer to document (FTF-SNT-F1121.pdf) of QorIQ (LS1).
   If the IP of PCIe of i.MX 6 and QorIQ (LS1) are the same, we can refer to the attached data.

    Is the IP same or not?

B.Regards,

Labels (1)
0 Kudos
1 Reply

939 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tomohisa

1. please create service request :
https://community.freescale.com/docs/DOC-329745

2. I am afraid IP of PCIe of i.MX 6 and QorIQ (LS1) is not the same.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos