Cannot find ZPS configuration editor for JN5179 in LPCXpresso_7.9.2_493

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot find ZPS configuration editor for JN5179 in LPCXpresso_7.9.2_493

2,061 Views
benjaminchang
Contributor V

Hi All,

I'm developing ZB30 application for JN5179, and want to use ZPS configuration editor as JN-UG-3113 described - to found it under "Jennic option". But I cannot find it in "LPCXpresso_7.9.2_493"

pastedImage_2.png

I have installed the newest JN-SW-4263 and 4270 as below.

Can you make a suggestion where is the problem? Thanks!

pastedImage_1.png

In "JN-RN-0062-JN-SW-4270-JN517x-ZigBee3-SDK.pdf" (v1520) says:

Software Component contains "ZPS Configuration Plug-ins  [v31504]". So where can we find it?

Thank you,

Benjamin

Labels (1)
3 Replies

1,295 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Benajmin,

-Please follow the path Help > Install New Software….

-In the Available Software screen, click the Add… button. The following Add Respository window will be displayed.

-In the Add Repository window:

pastedImage_1.png

file:/C:\NXP\LPCXpresso_7.9.2_493\lpcxpresso\sdk\JN-SW-4270\Tools\Eclipse_plugins\com.nxp.sdk.update...

-In the Available Software screen, expand Jennic ZBPro SDK and ensure that the checkboxes for Jennic RTOS Configuration Editor and Jennic ZBPro Configuration Editor are ticked. Click Next > to continue

-Continue following the step 6

1.2.3 Installing the ZigBee Plug-ins

http://www.nxp.com/documents/user_manual/JN-UG-3098.pdf?fsrch=1&sr=1&pageNum=1 

Hope it helps,

Mario

1,295 Views
benjaminchang
Contributor V

Hello Mario,

It works and got as below wizard. Thank you!

pastedImage_2.png

It is the same procedure as Danny described in Section 1.2.2 of JN-UG-3109.

Just wondering why my previous installation of JN-SW-4270 did not include this? I rember to have followed Section 3.2 "SDK Plug-in Installation" of "JN-RN-0062-JN-SW-4270-JN517x-ZigBee3-SDK.pdf", but only to found "All items are installed" message displayed under "NXP RFCS JN-SW-4270 Software Development Kit".

Thank you,

Benjamin

0 Kudos

1,295 Views
daniel_watson
NXP Employee
NXP Employee

Hi Benjamin,

*EDITED - Wrong Document. Below is now correct*

Please following the document below at section 1.2.2

http://www.nxp.com/documents/user_manual/JN-UG-3109.pdf 

Danny.

0 Kudos