AnsweredAssumed Answered

MKW01 RF not moving to TX mode

Question asked by Saurabh Jhamb on Apr 12, 2017
Latest reply on May 18, 2017 by Gerardo Rodríguez

Hi Folks,

 

I am trying to set up RF transmit in Kinetis MKW01Z128CHN.

The fixed packet length is set to 5 bytes and TxStartCondition is set to FifoLevel.

FifoLevel IRQ bit (in MKW01_Reg_IrqFlags2) is getting set properly after filling FIFO to full.

Then, when I try to move it to TX Mode by setting Mode bits in MKW01_Reg_OpMode, it does NOT set the ModeReady and TXReady status bits in MKW01_Reg_IrqFlags1.

 

MKW01_Reg_IrqFlags1 always reads 0, has anyone else faced this issue?

I am working on NXP Reference Design Board (MRB-KW0x)

 

Appreciate any help/pointers in achieving a simple Transmit/Receive setup.

Outcomes