Hi all,
I am testing with the LS1043ARDB-PB EVM board.
The AQR105-B1 has SPI Flash (MX25V4006E) memory,
It seems that 10G PHY does not work when memory is removed.
Do I need to write data to SPI Flash?
How can I write if I need to?
Is it possible on u-boot?
Thank you.
Best regards,
gyosun.
Is FMAN microcode loaded on your board?
Look at the Section 4.4.7.4 of the SDK 2.0-1703 Documentation:
http://www.nxp.com/assets/documents/data/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------