OTA support in JN-AN-1220

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OTA support in JN-AN-1220

525 Views
benjaminchang
Contributor V

We are using JN5179, and try to add OTA support in JN-AN-1220.

in section 5.7.2.1 "Using Makefiles" mentioned to add "OTA=1 to build with OTA client". But the whole project contains no OTA related files and very few words of OTA. Only one line "#APP_CLUSTERS_OTA_SRC ?=1" can be found in each makefile under directory build.

Please check if this JN-AN-1220 v1002 release really contains OTA support or not? Looks to me is NOT.

Thanks!

Tags (3)
0 Kudos
1 Reply

277 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Benjamin,

Your local sales will be in touch with you for solve this issue.

Regards,

Mario

0 Kudos