AH1310- Application hints

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AH1310- Application hints

1,479 Views
lipingren
Contributor I

Hi NXP customer support,

I have a question regarding AH1310- Application hints of “TJA1100 Automotive Ethernet PHY”. Section 3.4.5 Common mode termination on Page 18 indicates that “To provide some common mode termination of the channel, a split termination consisting of two resistors and a capacitor can be optionally connected to the signal lines between the coupling capacitors and the connector. For symmetry reasons the tolerance of the two resistors shall be within ±1%. The power rating of the resistors should be higher than 0.4W, depending on expected RF power in the actual application.”

I wonder larger than 0.4W specified here for resistor is the DC power or under AC. Why this power is needed?

Thanks,

Liping

0 Kudos
0 Replies