i.MX7 and Qt5.8 QtWebEngine

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX7 and Qt5.8 QtWebEngine

796 Views
ryanschaefer
Contributor IV

Is there a working example of the QtWebEngine on the i.MX7? I am unable to get the Qt provided demo browser to work on the i.mx7. With Qt5.8 including the Qt 2D renderer, it seems as though the QtWebEngine should be able to work without a gpu.

Labels (2)
0 Kudos
1 Reply

371 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Ryan,

Qt 5 works on SoCs without hardware graphics for Frame Buffer and X11 graphic backends only using mesa
software graphics, but it is not supported by official NXP Yocto BSP. You should take a look a third party development or Yocto community.

regards

0 Kudos