Jean-Michel Pedrono

Kinetis SDK 1.3.0 - FreeRTOS support?

Discussion created by Jean-Michel Pedrono on Apr 6, 2017
Latest reply on May 3, 2017 by Daniel Chen

Hello,

 

I want to play with FreeRTOS on my FRDM-K64F board.

 

I've installed Kinetis Design Studio 3.2.0 on my Ununtu 16.04 / 64bit (kinetis-design-studio_3.2.0-1_amd64.deb).

Then I've downloaded Kinetis DSK 1.3.0 Mainline, and registered it in KDS using "Install New Software".

 

I'm able to create, build and debug a default Kintetis SDK 1.x project.

 

Now, i want to add FreeRTOS to this project:

From "Component Library", i double-click FreeRTOS to add it to my project, but I'm getting the following error:

 

Error during adding referenced component/template "Unsupported/Utility-UNSUPPORTED".
Component is either missing or corrupted.

 

I probably did something wrong or forgot a step. Any idea?

 

Thanks.

Regards

Outcomes