Our customer use PN7462 for NFC reader, But the customer feedback, They have question of on SW_FW SDK(PN7462AU FW and SW Examples Full Version - v04_06_00), They found the SW will hang-up on phFlashBoot_HwInit() @ static void phFlashBoot_HwTearDown(void) . On the customer HW circuit, They have not the TDA8026 part.
Hi Ray,
So this is a custom board based on PN7462 , right? Which example was running on that board?
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Kan,
The HW design by customer, I helping customer to review the HW, I think the HW seem has some issue. Let’s me check and reply you later.
Thanks for you support.
Ray Cai
ray.cai@avnet.com<mailto:%20ray.cai@avnet.com>
Avnet Electronics Marketing
8/F,Block 2,Science Park Financial Base,8 Kefa Road, Hi-Tech Industrial Park, Nanshan, Shenzhen
深圳市南山区科技园科发路8号金融基地2栋8楼
M +86.18665998896
D +86 755 86342385
F +86 755 26544345 - 2385
avnet.com<http://avnet.com/>
发件人: Kan_Li
发送时间: 2017年4月11日 16:19
收件人: Cai, Ray <Ray.Cai@Avnet.com>
主题: Re: - Re: phFlashBoot_HwInit() problem of PN7462
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: phFlashBoot_HwInit() problem of PN7462
reply from Kan_Li<https://community.nxp.com/people/Kan_Li?et=watches.email.thread> in NFC - View the full discussion<https://community.nxp.com/message/895816?commentID=895816&et=watches.email.thread#comment-895816>