Hi,
We are using LS1043A, Kindly request you to confirm does this processor supports 10GBASE-KR?
Thanks.
Have a great day,
I see in the LS1043A manual that the SerDes module support:
"XFI/10GBASE-R @ 10.3125 Gbaud
IEEE Std 802.3ap-2007 Backplane Ethernet defines 3 PHY types
1000BASE-KX : 1-lane 1 Gb/s PHY (Clause 70)
10GBASE-KX4: 4-lane 10Gb/s PHY (Clause 71)
10GBASE-KR : 1-lane 10Gb/s PHY (Clause 72)
So support for XFI/10GBASE-R + IEEE 802.3ap-2007 means support for 10BASE-KR.
There is the LS1043A based mezzanine module XPedite6401 which claims support for the 10BASE-KR directly from the LS1043A. You can find its Block Diagram on the internet.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for your reply.
1. There is no electrical specification for 10GBase-KR in Manual or Datasheet. Can you please share with us?
2. Also Kindly let us know in LS1043A how to implement 10GBASE-KR using software or through any setting?
Thanks
I suggest you get IEEE 802.3ap-2007 documentation. It specifies 10GBASE-KR features related to the backplane Ethernet. Then create technical case to the nxp support for confirmation of the 10GBASE-KR features you need. Please see See How I could create a Service Request?