Hi,
Can any one help me in updating 2.6.20-kernel to higher version for the development board MPC8323E-RDB.? I am using MPC8323E-RDB board and I downloaded ISO image from nxp website. I built this with LTIB and finally I got the linux kernel with 2.6.20 version. In the progress of driver development of I am facing some issues with this versions for example that it not supporting some Kernel-APIs. I didn't find any other option for selecting other than 2.6.20 kernel while kernel configuration using LTIB.
Please, help in updating the kernel to higher supportive kernel to this development board.
Thanks and Regards,
Siva Prakash Reddy Narreddy
Look at information on the following pages
http://www.berkes.ca/guides/linux_kernel.html
http://www.bitshrine.org/autodocs/LtibFaq.html
https://freescale.jiveon.com/thread/28758
http://ltib.nongnu.narkive.com/8XSfiWTA/how-to-upgrade-the-kernel-to-2-6-21-on-mpc8349e-board
https://lists.gnu.org/archive/html/ltib/2011-11/msg00019.html
https://lists.gnu.org/archive/html/ltib/2007-07/msg00009.html
https://lists.nongnu.org/archive/html/ltib/2008-11/msg00013.html
See also the following:
http://ltib.org/pages/LTIB_generic_v1.4_-_version_6.4.1.pdf
http://www.nxp.com/assets/documents/data/en/application-notes/AN3765.pdf
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------