Hi,
Under the following conditions:
-. i.MX6 configured as PCIe RC
- The i.MX6 is connected to PCIe EP
- The EP wants to perform DMA write operation to the I.MX6 RAM
Does this scenario supported?
Thanks,
Eyal
Hello Eyal,
In EP's system, EP can access the reserved ddr memory (default address:0x40000000) of PCIe RC's system, by the interconnection between PCIe EP and PCIe RC. So I don´t see a problem.
Here is a link of a validation
i.MX6Q PCIe EP/RC Validation System
Have a great day,
Jaime
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------