error to compile the demo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

error to compile the demo

Jump to solution
1,844 Views
huaping
Contributor III

I follow the guide to open K64 SDK example, hello world demo, but failed to compile, pls help check it in the attached file.

0 Kudos
1 Solution
1,711 Views
andybeeson
NXP Employee
NXP Employee

What OS version are you using? It also looks like you may have changed the drive you installed the IDE onto from C: to D: correct?

Anyway, we've seen one similar case to this before with MCUXpresso IDE (though no reports with LPCXpresso IDE, which in this respect should be the same). That was solved by rebooting the PC...

https://community.nxp.com/thread/447847 

View solution in original post

2 Replies
1,712 Views
andybeeson
NXP Employee
NXP Employee

What OS version are you using? It also looks like you may have changed the drive you installed the IDE onto from C: to D: correct?

Anyway, we've seen one similar case to this before with MCUXpresso IDE (though no reports with LPCXpresso IDE, which in this respect should be the same). That was solved by rebooting the PC...

https://community.nxp.com/thread/447847 

1,711 Views
rastislav_pavlanin
NXP Employee
NXP Employee

Hello Tan,

did you follow all the instruction in the lab? attached doc file.

regards

R.

0 Kudos