Hi All:
I have some questions about the IMX6.
In the IMX6 reference manual chapter 60, table 60-3 power mode transitions “Normal to OFF, by button”, the alarm timer is set up by software routine and started.
1. Can I modify the alarm timer to become 10 sec? After 10 sec, the “PMIC_ON_REQ” goes “0”.
2. Can I modify the software not to start the alarm timer? Will the “PMIC_ON_REQ” not go “0”, if the software does not start the alarm timer?
3. Is the software rountine is provided by NXP? For example, in the demo board software.
Your help is appreciated.
Hi Igor:
Thanks for the response. Yes, I am using the external PMIC. How about my questions above? Is it possible to do that?
Best Regards
HT Lee
Hi Igor:
Thanks for the response. I am using the IMX6 Dual Lite. I do not quite understand your answer. Do you mean IMX6 does not support table 60-3 power mode transitions in dumb PMIC mode?
Hi HT
supported only configuration with external pmic
Best regards
igor
Hi HT
on i.MX6Q only DUMB PMIC option is supported.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------