Hello,
i have develop a new embedded board with the MK22FX512VLL12. I have put a pull-up of 10kohm on the reset pin but when i try to program this micro for the first time the reset pin continue to oscillate.
i have try with the segger commander with the command erase and unlock kinetis but nothing. I can't erase the memory. I have read some post that speak about this problem but i didn't find a solution. I use a EDU Segger Jlink.
This happen on all board
Thanks
Ok, for two board i have solve using jlink commander:
monday i will try with other board
Hi Daniel Cortellazzi
Actually this is not a problem, it is telling you that there is anything in the flash memory, so when your device try to fetch a instruction from the internal flash and it doesn't find anything it cause a hard fault and it reset, when the process repeat, it reset again, and it stock in this loop.
If you flash a program in this devices the reset line should behave normal.
Have a great day,
Jorge Alcala
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------