I have installed QT on Debian on iMX6ul. linux is new for me.
I have also control GPIO using command from bash.
$ echo 133 > /sys/class/gpio/export$ echo out > /sys/class/gpio/gpio133/direction$ echo 1 > /sys/class/gpio/gpio133/value //Pin high$ echo 0 > /sys/class/gpio/gpio133/value //Pin low
My problem is that, I want to communicate with peripheral like GPIO, Bluetooth, Wi-Fi, Ethernet etc from QT.
Which is best way to communicate with peripheral in QT from user application.
Thanks,
Jignesh Patel
Hi Jignesh
please check
Qt 4.6: Qt for Embedded Linux Character Input
controll led, button, GPIO with QT - FriendlyARM
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------