AnsweredAssumed Answered

UART for ISP

Question asked by prachipanse on Mar 29, 2017
Latest reply on Mar 30, 2017 by prachipanse

Hi,

 

I need to program the on-chip flash of LPC1313FBD48/01 device. I have connected the SWCLK and the SWDIO pins to the debug connector. The UART interface is connected to some other peripheral. I have some queries regarding the same:

Is it necessary to use ISP or IAP modes to program the flash or can it be done without that?

Also, if ISP mode is to be used, how is the UART interface to be used for this purpose?

 

Thanks and Regards,

Prachi

Outcomes