AnsweredAssumed Answered

interrupt cells of i.MX6 in devicetree

Question asked by Zongbiao Liao on Mar 28, 2017
Latest reply on Mar 28, 2017 by igorpadykov

Hello Community

 

in linux4.1.15/Documentation/devicetree/bindings/interrupt-controller/interruputs.txt, it only explains the meaning of interrupt specifier with one cell and two cells.

But in imx6qdl.dtsi, interrupt specifier has three cells, for example:

----------

src: src@020d8000 {
compatible = "fsl,imx6q-src", "fsl,imx51-src";
reg = <0x020d8000 0x4000>;
interrupts = <0 91 IRQ_TYPE_LEVEL_HIGH>,
<0 96 IRQ_TYPE_LEVEL_HIGH>;
#reset-cells = <1>;
};

-----------

 

I understood that the second cell means index of the interrupt and the third cell specifies trigger type and level flags.

What does the first cell mean.

Does it mean: 1-irq masked and 0-irq is not masked ?

 

Best Regards

ZongbiaoLiao

Outcomes