OTA Firmware upgrade over IMX6 solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OTA Firmware upgrade over IMX6 solo

1,180 Views
adityanagal
Contributor III

Hi ,

I am working over the IMX6 solo and need to develop Firmware upgrade OTA . In which boot mode , processor need to boot up to support Firmware upgrade. Please suggest.

Regards,

Aditya Nagal

0 Kudos
1 Reply

730 Views
igorpadykov
NXP Employee
NXP Employee

Hi Aditya

from hardware point of view there is no special ota mode, it

may be useful to check Android documentation on

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

please check p.7 attached Android User's Guide

sect.30 How do I build an OTA package? Android Frequently Asked Questions

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos