How to unsecure MC9S12GA192 microcontroller?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to unsecure MC9S12GA192 microcontroller?

Jump to solution
1,067 Views
amitdhand
Contributor I

I have been working on the hcs12 microcontroller part number mc9s12ga192. I flashed the microcontroller with wrong configuration and the microcontroller went to secure mode. Now what would be the procedure to unsecure it.

Please help out.

0 Kudos
1 Solution
738 Views
RadekS
NXP Employee
NXP Employee

Hi Amit,

The CW debugger offers Unsecure per used debugger probe.

If you use PEmicro interfaces like USB Multilink, CyclonePro or OSBDM please go to CW debugger menu ->MultilinkCyclonePro->Unsecure…

The FCLKDIV value for default S12G clock should be selected 6.

If it not works you can use unsecure12 from P&E:

http://www.pemicro.com/downloads/download_file.cfm?download_id=16

 

More details about S12(X) security:

https://community.nxp.com/docs/DOC-93803

I hope it helps you.

Have a great day,
Radek
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
739 Views
RadekS
NXP Employee
NXP Employee

Hi Amit,

The CW debugger offers Unsecure per used debugger probe.

If you use PEmicro interfaces like USB Multilink, CyclonePro or OSBDM please go to CW debugger menu ->MultilinkCyclonePro->Unsecure…

The FCLKDIV value for default S12G clock should be selected 6.

If it not works you can use unsecure12 from P&E:

http://www.pemicro.com/downloads/download_file.cfm?download_id=16

 

More details about S12(X) security:

https://community.nxp.com/docs/DOC-93803

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos