Unable to fetch the resource from the link - git.projects.genivi.org/wayland-ivi-extension.git. Help me.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to fetch the resource from the link - git.projects.genivi.org/wayland-ivi-extension.git. Help me.

1,176 Views
ponguru_s
Contributor III

Hi,

I’m working on i.MX 6Q Sabre Automotive (i.mx 6q sabreauto). I’m following the same procedure mentioned in the Readme.txt for NXP AGL 4.1.15 – 1.0.0 from the link below.

http://git.freescale.com/git/cgit.cgi/imx/meta-nxp-agl.git

http://git.freescale.com/git/cgit.cgi/imx/meta-nxp-agl.git/tree/README.txt?id=jethro-4.1.15-1.0.0

 

Initially, I got the error mentioned below.

 

ERROR: ExpansionError during parsing /media/mynewdrive/NXPAGL_4_1_15_jethro/sources/meta-agl-demo/recipes-demo-hmi/CES2016-demo/CES2016-demo.bb: Failure expanding variable SRCPV, expression was ${@bb.fetch2.get_srcrev(d)} which triggered exception FetchError: Fetcher failure: Fetch command failed with exit code 128, output:

fatal: repository 'https://gerrit.automotivelinux.org/AGL/DemoApps/CES2016/' not found

 

I modified the sources/meta-agl-demo/recipes-demo-hmi/CES2016-demo/CES2016-demo.bb file mentioned, as follows.

 

#SRC_URI     = "git://git.automotivelinux.org/gerrit/AGL/DemoApps/CES2016;protocol=http"

SRC_URI = "git://git.automotivelinux.org/AGL/DemoApps/CES2016;protocol=https”    /*Modification*/

 

This modification rectified the error and it showed up one more error, as shown below. In the .bb file mentioned in the error, it is unable to fetch wayland-ivi-extension.git from the URL git2/git.projects.genivi.org.

 

ERROR: Fetcher failure: Fetch command failed with exit code 128, output:

Cloning into bare repository '/media/mynewdrive/NXPAGL_4_1_15_jethro/downloads//git2/git.projects.genivi.org.wayland-ivi-extension.git'...

fatal: remote error: access denied or repository not exported: /wayland-ivi-extension.git

 

ERROR: Function failed: Fetcher failure for URL: 'git://git.projects.genivi.org/wayland-ivi-extension.git'. Unable to fetch URL from any source.

ERROR: Logfile of failure stored in: /media/mynewdrive/NXPAGL_4_1_15_jethro/bld-agl/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/wayland-ivi-extension/1.5.0-r0/temp/log.do_fetch.30105

ERROR: Task 2890 (/media/mynewdrive/NXPAGL_4_1_15_jethro/sources/meta-agl/meta-ivi-common/recipes-graphics/wayland/wayland-ivi-extension_1.5.0.bb, do_fetch) failed with exit code '1'

 

Please provide me a solution to proceed further, at the earliest possible.

1 Reply

544 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Surendranath Ponguru,

Have you tried following the instructions on the following document?

Build Genivi for i.MX6 

It is possible that repositories have changed. Please let us know if the steps on the document fail.

Regards,