For NOR or NAND the buffer is controlled by IFC_TE (enable) and IFC_BCTL (direction) signals?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

For NOR or NAND the buffer is controlled by IFC_TE (enable) and IFC_BCTL (direction) signals?

715 Views
tracysmith
Contributor IV

How is IFC-TE, IFC_BCTL, and IFC_CLK0 being used in u-boot and the kernel for the IFC? 

If IFC_BCTL and IFC_CLK0 for the IFC is removed on a custom board, what are the implications for SDK 2.0 and the LS1043ARDB?

Labels (1)
Tags (1)
0 Kudos
1 Reply

522 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

The u-boot/kernel IFC driver should take into account using IFC_TE pin and sets the TE bit in the Chip-select Property register properly. While used IFC_BCTL signal should be enabled in the Chip-Select Option register.

Unused IFC_BCTL and IFC_CLK0 output signals do not require any u-boot/kernel software modifications.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos