sgmii configuration in p1022

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sgmii configuration in p1022

481 Views
somyaaggarwal08
Contributor II

Hi,

I want to configure sgmii interface in p1022 based card from uboot. Could any suggest what all changes need to be done in order to enable so. By default etsec mode is enabled

Labels (1)
0 Kudos
2 Replies

343 Views
Pavel
NXP Employee
NXP Employee

The P1022ds u-boot provides SGMII connection automatically. See attached file. It is tsec driver from NXP SDK 1.9. Find the init_phy procedure in this file.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

343 Views
somyaaggarwal08
Contributor II

Hi Pavel

Thank you for the above information

0 Kudos