i.MX6 Solo, Dual lite and Quad in same design with 1/2/4GB RAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 Solo, Dual lite and Quad in same design with 1/2/4GB RAM

1,815 Views
rahulsoni
Contributor II

Hi Folks,

We are designing a board based on SabreSD. We are planning to use all, i.MX6 Solo, Dual-lite and Quad processor on the same board with 1GB, 2GB, and 4GB DDR3 RAM respectively while the PCB remains same for all the three configurations.

When using i.MX6 Quad, we'll mount four 8Gb DDR3 (MT41K512M16HA-125 IT).

In case of i.MX6 Dual-lite, we'll mount two 8Gb DDR3 (MT41K512M16HA-125 IT) &

In case of i.MX6 Solo, we'll mount single 8Gb DDR3 (MT41K512M16HA-125 IT).

In the reference layout (LAY-27392_C), balanced T topology has been used for connecting all 4 DDR3 RAMs back to back. 

I would like to know if I should go with fly-by topology or balanced T topology as in the case of balanced T topology when 3 RAMs are not mounted (with i.MX Solo configuration). Will there be any effect of noise due to the stubs in the absence of other 3 RAMs?

Also, do let me know what precautions to be taken care while migrating from quad to dual lite and solo processor. I have referred to Application Note AN4397 for schematics design.

Any help is appreciated@ in advance.igorpadykov

 

 

0 Kudos
2 Replies

1,199 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rahul

one can check sect.3.6 i.MX6 System Development User’s Guide for fly-by topology

and enter service request for obtaining i.MX6Q design example

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

Yes, one can expect noise due to the stubs, as mentioned in AN4397

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,199 Views
rahulsoni
Contributor II

Do let me know what precautions to be taken care while migrating from quad to dual lite and solo processor. I have referred to Application Note AN4397 for schematics design.

What else should I take care of?

0 Kudos