FATAL ERROR when reading from P4080 on PCIe

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FATAL ERROR when reading from P4080 on PCIe

Jump to solution
632 Views
emilhjalmarsson
Contributor I

Hi,

We have a system where an FPGA and a P4080 is connected to a PCIe switch. The FPGA reads/writes from the CPU.

We recently decided to go from 128 bytes packets to 256 bytes on the PCIe and now it doesn't work anymore.

It works fine when the FPGA writes to the CPU but when is sends a Memory Read Request is casuses a FATAL ERROR in the CPU. Bit FEMR, FUF, MEFNFR and EFNFR in Root_Error_Status_Register are set.

The TLP Header sent to the CPU is 20000040'h which means Memory Read Request (4DW, no data) and 256 bytes of data.

MAX_PAYLOAD_SIZE in the switch are set to 256 bytes on both ports in the switch.

MAX_READ_SIZE in Device_Control_Register are set to "010" and MAX_PAYLOAD_SIZE in Device_Control_Register are set to "001".

Am I missing something?

Regards

/Emil

Labels (1)
0 Kudos
1 Solution
452 Views
ufedor
NXP Employee
NXP Employee

It will be convenient to investigate the issue as a Technical Case:

https://community.freescale.com/thread/381898

View solution in original post

0 Kudos
1 Reply
453 Views
ufedor
NXP Employee
NXP Employee

It will be convenient to investigate the issue as a Technical Case:

https://community.freescale.com/thread/381898

0 Kudos