The register of MPC5746R i.e DMA/Interrupt Request Select and Enable Register (DSPI_RSER) does not show any values after flashing the code. What configuration is to be done in Eb-Tresos to get value to that register?
If there is no configuration related to that register, should we write manual code for it? if yes, then that code should be written in the Spi code or should be in the related module?
If it can be configured in Eb-tresos then is it violating autosar rules?
Hi,
Register should be configured according to selected transfer, interrupt driven or DMA driven.
Peter