I have been using the LPC1549, when i do firmware upgrades on this device i simply connect the device to a USB port and my PC sees the device as a MSC, i can then copy the bin file straight to the MSC.
This feature is very useful for firmware upgrades on site where the technicians do not need any special tools or applications.
Is this feature available on the LPC1837 / LPC1857?
Thanks
1)Is this feature available on the LPC1837 / LPC1857?
No, these chips don't support.
Have a great day,
Ping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------