Embedded Trace Macrocell (ETM) PCB Routing Tips

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Embedded Trace Macrocell (ETM) PCB Routing Tips

1,256 Views
pgvoorhees
Contributor II

Hello Community,

We are planning on using ETM to aid in debugging but have found very few routing guidelines for the TRACE_D[0:3] and TRACE_CLK nets.

On the K22FX512, using a 120MHz core speed, What is:

  • The clock speed of the TRACE nets? Datasheet says the interface is limited to 50MHz but offers no guidance for determining the speed.
  • Is any particular characteristic impedance for the traces necessary?
  • Do the lines need to be length-matched?

Design guild-lines seem to be largely unavailable and the Kinetis datasheets are light on details for this particular functionality. Any help is appreciated. Thanks!

Labels (1)
0 Kudos
1 Reply

932 Views
pgvoorhees
Contributor II

The best reference I've found for this is the Segger J-Link/J-Trace manual.

J-Link Debug Probes | SEGGER - The Embedded Experts 

Chapter 17 (as of this post) called "Designing the target board for trace"

0 Kudos