AnsweredAssumed Answered

i.mx solox boot from QSPI1B

Question asked by Asaf Elias on Mar 15, 2017
Latest reply on Mar 15, 2017 by igorpadykov

Hey

I have a custom board with an i.mx 6sx which is based on the sabresd desgin.

I've connected a n25Q256a QSPI device to QSPI 1B.

Is it possible to boot from this device? 

In my tests i see that on POR (or with bmode) only the QSPI 1A or QSPI2A are accessed be the boot ROM.

also, the fuses / GPIOS can only be configured for QSPI1 or QSPI2 and does not give an option to configure A or B inside a specific controller.

 

Thank you

Asaf

Outcomes