AnsweredAssumed Answered

10 Bit Monochrome CMOS Image Sensor Interface.

Question asked by Harish S on Mar 14, 2017
Latest reply on Mar 21, 2017 by Joan Xie
Branched to a new discussion

Hi,

 

Our application needs interfacing a 10 Bit Monochrome CMOS image sensor(EV76C661ABTF) parallely to i.MX 6 processor.

Since IPU Sensor Interface of i.MX6 supports upto 20 Bit camera interface,need help on interfacing the Image sensor.

 

From the Table 62 .Camera Input Signal Cross Reference, Format, and Bits Per Cycle given at page 95 of datasheet, I am not getting a clear picture about a grey scale format pin mapping to i.MX 6.

 

Also need some clarification on input clock required for image sensor, since the CSI0_MCLK CLK provided is multiplexed with CSI0_HSYNC  and no other alternate pin is available.

 

Attached the datasheet of Image sensor and I.MX 6 processor for reference.

 

Regards,

Harish.S

Outcomes