Hello,
i want to program my FXTH87 sensor. I know the programming interface to this is BDM connector from P & E . But it requires the BDM connector along with the debugger. Is there a way to program this without having to use the BDM connector?
Hello Prashant,
Thank you very much for writing.
In this case, the FXTH87 has an S08, 8-bit microprocessor core, therefore you would require a universal BDM and CodeWarrior to program it.
I would recommend you the following BDM interface.
Please note that the BDM is open source, so you can implement your own programmer.
OSBDM is an open source hardware/software/firmware design which provides low-speed debug communications for different NXP processors. It is embedded within many of NXP’s development board and tower cards.
Please find more information at:
https://www.pemicro.com/osbdm/osbdm_description.cfm
I hope this information helps.
Best Regards,
David
Hello David,
Thanks for the info.