SD_CD Pin in i.Mx7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SD_CD Pin in i.Mx7

458 Views
meriajacob
Contributor I

Hi,

The SD card is not detected in our board after power up. In our schematics, we have assigned the SD_CD pin to No Connect. We use the micro controller MCIMX7D7DVM10SC

But when we go in detail through the user manual its written, for embedded memory it should be tied to ground if not used. Will this cause an issue?

Kindly share your thoughts in this regard!!!!

Thanks,
Regards,
Meria Jacob

Labels (2)
0 Kudos
1 Reply

353 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Meria,

Yes, this is a problem if you do not have this pin in a low level,  it is never going to generate the proper interrupt event to detect the SD Card.  An option can be enable the pulldown resistor internally of the PAD.  and test.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos