AnsweredAssumed Answered

PN7150 - HardFault_Handler problem

Question asked by Adrian Pakosiński on Mar 9, 2017
Latest reply on Mar 23, 2017 by davidwatzinger

Hello,

 

I try to run example for the PN7150 chip. Unfortunately, the program stops in the function HardFault_Handler. I didn't make changes in the example project. I used the instructions from application note: AN11658.

 

Hardware:

OM5578/PN7150ARD

LPC1114 LPCXpresso board

 

Software:

LPCXpresso v8.2.2 [Build 650]

NXP-NCI LPCXpresso example (SW3241) - NXP-NCI_LPC11xx_example

 

What do you think could be wrong ? Maybe something should be changed in the project properties ? I checked the connections between boards and I think that are correct.

 

Best Regards,

Adrian Pakosinski

 

Outcomes