Hi ,
I am trying to decode the AAC audio file using the following pipeline. But it is giving the error. Could somebody please suggest me the correct pipeline to decode the AAC file.
gst-launch-1.0 filesrc location=/mnt/Audio_Files/sample.aac ! imxuniaudiodec ! alsasink device="hw:0,0"
Error output :
Setting pipeline to PAUSED ...
Pipeline is PREROLLING ...
ERROR: from element /GstPipeline:pipeline0/GstFileSrc:filesrc0: Internal data flow error.
Additional debug info:
gstbasesrc.c(2948): gst_base_src_loop (): /GstPipeline:pipeline0/GstFileSrc:filesrc0:
streaming task paused, reason error (-5)
ERROR: pipeline doesn't want to preroll.
Setting pipeline to NULL ...
Freeing pipeline ...
What will be the correct pipeline ?
Thanks,
Aditya Nagal
Hi,
I encountered the same issue with this pipeline:
gst-launch-1.0 filesrc location=/home/root/ten.mp3 ! imxuniaudiodec ! audioconvert ! autoaudiosink name=audiosink
Could you find the correct pipeline ?
regards,
étienne
Hi Aditya
imxuniaudiodec is part of community gstreamer-imx plugins described on
trac.gateworks.com/wiki/Yocto/gstreamer
one can post on to meta-fsl-arm mailing list, so that someone familiar with it could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale
or check similar issue
libimxvpuapi wayland sink issue
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------